Part Number: AM3352
Other Parts Discussed in Thread: AM3358
Hello,
We are using linux kernel 4.4.32 on custom board having AM3352. We observed that boot process is taking too much time after the print "Starting kernel..." .
Booting hangs here for 10 seconds and the next prints of kernel starts.
In between boot process we are receiving below print for different 3-4 times, and it hangs for 6-7 seconds each time:
[ ***] (2 of 2) A start job is running for Login Service (59s / 2min 8s)[ 65.317937]
Below is the full boot log:
U-Boot SPL 2017.01 (Apr 12 2018 - 12:01:11)
Trying to boot from MMC2
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2017.01 (Apr 12 2018 - 12:01:11 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3857280 bytes read in 775 ms (4.7 MiB/s)
36283 bytes read in 29 ms (1.2 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff4000, end 8ffffdba ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.32-gc779b97590 (einfochips@AHMLPT0458) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #7 PREEMPT Wed A
pr 25 18:52:33 IST 2018
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 48 MiB at 0xbd000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260416
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 978344K/1048576K available (7447K kernel code, 336K rwdata, 2492K rodata, 268K init, 292K bss, 21080K reserved, 49152K c
ma-reserved, 212992K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc09bcfec (9940 kB)
[ 0.000000] .init : 0xc09bd000 - 0xc0a00000 ( 268 kB)
[ 0.000000] .data : 0xc0a00000 - 0xc0a54030 ( 337 kB)
[ 0.000000] .bss : 0xc0a54030 - 0xc0a9d33c ( 293 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000028] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000074] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000098] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000452] clocksource_probe: no matching clocksources found
[ 0.000786] Console: colour dummy device 80x30
[ 0.000843] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992)
[ 0.067815] pid_max: default: 32768 minimum: 301
[ 0.068048] Security Framework initialized
[ 0.068144] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.068173] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.069677] Initializing cgroup subsys io
[ 0.069738] Initializing cgroup subsys memory
[ 0.069810] Initializing cgroup subsys devices
[ 0.069842] Initializing cgroup subsys freezer
[ 0.069872] Initializing cgroup subsys perf_event
[ 0.069900] Initializing cgroup subsys pids
[ 0.069960] CPU: Testing write buffer coherency: ok
[ 0.070696] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.075882] devtmpfs: initialized
[ 0.104764] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.136243] omap_hwmod: debugss: _wait_target_disable failed
[ 0.199619] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.207092] pinctrl core: initialized pinctrl subsystem
[ 0.210232] NET: Registered protocol family 16
[ 0.214965] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.237906] cpuidle: using governor ladder
[ 0.267888] cpuidle: using governor menu
[ 0.278646] OMAP GPIO hardware version 0.1
[ 0.303207] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.368451] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.378430] SCSI subsystem initialized
[ 0.379438] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring p
robe
[ 0.379812] pps_core: LinuxPPS API ver. 1 registered
[ 0.379836] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.379916] PTP clock support registered
[ 0.380063] EDAC MC: Ver: 3.0.0
[ 0.382567] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.384669] Bluetooth: Core ver 2.21
[ 0.384782] NET: Registered protocol family 31
[ 0.384802] Bluetooth: HCI device and connection manager initialized
[ 0.384837] Bluetooth: HCI socket layer initialized
[ 0.384866] Bluetooth: L2CAP socket layer initialized
[ 0.384961] Bluetooth: SCO socket layer initialized
[ 0.387323] clocksource: Switched to clocksource timer1
[ 0.414062] NET: Registered protocol family 2
[ 0.415729] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.415960] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.416179] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.416394] UDP hash table entries: 512 (order: 1, 8192 bytes)
[ 0.416465] UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
[ 0.416816] NET: Registered protocol family 1
[ 0.417708] RPC: Registered named UNIX socket transport module.
[ 0.417741] RPC: Registered udp transport module.
[ 0.417757] RPC: Registered tcp transport module.
[ 0.417773] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.419217] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.423733] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.445309] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.449779] NFS: Registering the id_resolver key type
[ 0.449938] Key type id_resolver registered
[ 0.449957] Key type id_legacy registered
[ 0.450137] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.481530] bounce: pool size: 64 pages
[ 0.482116] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[ 0.482171] io scheduler noop registered
[ 0.482208] io scheduler deadline registered
[ 0.482310] io scheduler cfq registered (default)
[ 0.484915] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.649405] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.658494] omap_uart 44e09000.serial: no wakeirq for uart0
[ 0.658931] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a OMAP UART0
[ 1.303289] console [ttyO0] enabled
[ 1.308225] omap_uart 48024000.serial: no wakeirq for uart2
[ 1.314591] 48024000.serial: ttyO2 at MMIO 0x48024000 (irq = 159, base_baud = 3000000) is a OMAP UART2
[ 1.325619] omap_uart 481a6000.serial: no wakeirq for uart3
[ 1.331910] 481a6000.serial: ttyO3 at MMIO 0x481a6000 (irq = 160, base_baud = 3000000) is a OMAP UART3
[ 1.342885] omap_uart 481a8000.serial: no wakeirq for uart4
[ 1.349166] 481a8000.serial: ttyO4 at MMIO 0x481a8000 (irq = 161, base_baud = 3000000) is a OMAP UART4
[ 1.360217] [drm] Initialized drm 1.1.0 20060810
[ 1.383335] loop: module loaded
[ 1.395113] libphy: Fixed MDIO Bus: probed
[ 1.402075] ksz8863 spi1.0: chip id 0x8831
[ 1.409731] libphy: Switch MII bus: probed
[ 1.443180] ksz8863: 0xC6(198) ->0xA
[ 1.467166] cpsw 4a100000.ethernet: No slave[1] phy_id, phy-handle, or fixed-link property
[ 1.476170] cpsw 4a100000.ethernet: Detected MACID = f4:5e:ab:39:6c:6c
[ 1.498812] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.509011] mousedev: PS/2 mouse device common for all mice
[ 1.516424] i2c /dev entries driver
[ 1.524188] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.531899] Bluetooth: HCI UART driver ver 2.3
[ 1.536632] Bluetooth: HCI UART protocol LL registered
[ 1.543045] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.551908] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.678793] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.693122] mmc0: new high speed SDHC card at address aaaa
[ 1.700271] mmcblk0: mmc0:aaaa SL16G 14.8 GiB
[ 1.712828] mmcblk0: p1 p2 p3 p4 < p5 p6 >
[ 1.759783] nf_conntrack version 0.5.0 (16054 buckets, 64216 max)
[ 1.766493] mmc1: MAN_BKOPS_EN bit is not set
[ 1.774453] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.780392] mmc1: new high speed MMC card at address 0001
[ 1.788930] NET: Registered protocol family 10
[ 1.795442] mmcblk1: mmc1:0001 W62704 3.56 GiB
[ 1.802189] sit: IPv6 over IPv4 tunneling driver
[ 1.807903] mmcblk1boot0: mmc1:0001 W62704 partition 1 2.00 MiB
[ 1.815962] NET: Registered protocol family 17
[ 1.821486] mmcblk1boot1: mmc1:0001 W62704 partition 2 2.00 MiB
[ 1.828056] bridge: automatic filtering via arp/ip/ip6tables has been deprecated. Update your scripts to load br_netfilter if you need this.
[ 1.843421] Bluetooth: RFCOMM TTY layer initialized
[ 1.848964] mmcblk1: p1 p2
[ 1.856093] Bluetooth: RFCOMM socket layer initialized
[ 1.862826] Bluetooth: RFCOMM ver 1.11
[ 1.867070] 8021q: 802.1Q VLAN Support v1.8
[ 1.875365] Key type dns_resolver registered
[ 1.880407] omap_hsmmc 47810000.mmc: card claims to support voltages below defined range
[ 1.889085] omap_voltage_late_init: Voltage driver support not added
[ 1.898408] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 600000 KHz
[ 1.906302] cpu cpu0: dev_pm_opp_domain_set_rate: failed to find current OPP for freq 600000000 (-34)
[ 1.916428] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 300000 KHz
[ 1.938856] mmc2: queuing unknown CIS tuple 0x91 (3 bytes)
[ 1.952973] mmc2: new SDIO card at address 0001
[ 1.962949] rtc-pcf8563 2-0051: chip found, driver version 0.4.4
[ 1.995899] rtc-pcf8563 2-0051: rtc core: registered rtc-pcf8563 as rtc0
[ 2.004610] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 2.014579] rtc-pcf8563 2-0051: setting system clock to 2018-04-25 07:01:07 UTC (1524639667)
[ 2.047662] sw-ksz8863: disabling
[ 2.079931] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.089147] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.107066] devtmpfs: mounted
[ 2.112767] Freeing unused kernel memory: 268K (c09bd000 - c0a00000)
[ 2.119722] This architecture does not have kernel memory protection.
[ 2.566150] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 2.590218] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
[ 2.655134] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRY
PT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 2.677238] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 2.713502] systemd[1]: Set hostname to <am335x-evm>.
[ 3.084846] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.133501] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.154406] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.218274] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
[ 3.360323] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 3.378454] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 3.391399] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 3.406797] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 5.396542] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.419854] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.449550] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.478565] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.518263] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 5.556099] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 5.615279] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.693755] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 5.750184] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.779103] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.809795] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 5.843633] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 5.894515] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 5.939953] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 6.036881] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.102228] cryptodev: driver 1.8 loaded.
[ 6.192228] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 6.321882] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.541230] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 6.620395] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 6.709796] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 6.799940] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pi[ 6.895457] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
pe.
[ 6.919439] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 6.979255] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 7.074953] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 7.241453] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 8.748207] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 8.778950] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 8.808773] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 8.841058] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Setup Virtual Console.
Starting udev Coldplug all Devices...
Mounting Configuration File System...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted Configuration File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ 18.144455] systemd-journald[104]: Received request to flush runtime journal from PID 1
[ 18.157616] random: nonblocking pool is initialized
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
[ 24.435832] TI-am335x-tsc TI-am335x-tsc: ti,charge-delay not specified
[ 24.599703] input: ti-tsc as /devices/platform/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input0
[ 26.593798] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 26.805977] wlcore: loaded
[ OK ] Found device /dev/ttyO0.
[ 29.144830] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 30.613001] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
Starting Load/Save RF Kill Switch Status...
[ OK ] Started Load/Save RF Kill Switch Status.
[ OK ] Started Network Time Synchronization.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Reached target System Time Synchronized.
Starting Synchronize System and HW clocks...
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Reached target System Initialization.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Permit User Sessions...
[ OK ] Started System Logging Service.
Starting Telephony service...
[ OK ] Started A userspace daemon that run... under the eCryptfs mount point.
[ OK ] Started Kernel Logging Service.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Telephony service.
Starting Network Service...
Starting Login Service...
[ OK ] Started Permit User Sessions.
[ OK ] Started Network Service.
[ 51.577877] wlcore: firmware booted (Rev 6.3.10.0.133)
[ 51.758889] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 51.957964] net eth0: initializing cpsw version 1.12 (0)
[ 51.963753] net eth0: initialized cpsw ale version 1.4
[ 52.013564] net eth0: ALE Table size 1024
[ 52.107861] net eth0: phy found : id is : 0x0
[ 52.112838] libphy: PHY not found
[ 52.116535] net eth0: phy "" not found on slave 1, err -19
[ 52.223441] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 52.277819] 8021q: adding VLAN 0 to HW filter on device eth0
[ 54.107888] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
[ 54.116405] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ OK ] Reached target Network.
Starting Network Name Resolution...
Starting Network Time Service...
Starting LLDP daemon...
Starting Lightning Fast Webserver With Light System Requirements...
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyO0.
[ OK ] Started LLDP daemon.
[ OK ] Started Network Time Service.
[ OK ] Started Login Service.
[ OK ] Started Network Name Resolution.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2016.12 am335x-evm ttyO0
am335x-evm login: root
Thanks,
Rohit