This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: ADC FSM_BUSY recovery

Part Number: AM3354


Hi,

Our customer is using TSC_ADC to control touchscreen.
Sometimes FSM_BUSY occurs and TSC_ADC hangs.

After the occurrence of FSM_BUSY, if the following processing is executed, it returned normally but is it correct as processing?

① Set the enable bit of the CTRL register to 0.
② Resetting the STEPENABLE register
③ Set the enable bit of the CTRL register to 1.

In the answer of the following e2e site, the answer was that the recovery process had only hardware reset.
e2e.ti.com/.../555302
http://e2e.ti.com/support/arm/sitara_arm/f/791/t/596863

Best Regards,
Shigehiro Tsuda

  • Part Number: AM3354

    Hi,

    FSM_BUSY no longer occurs after source changing to the following interrupt processing.
    Is it the correct process?

    --------------------------------------------------------------------------------------
    before
    am335xOutLong(TSC_ADC_IRQSTATUS, (1 << 5)); /* int clear*/
    am335xOutLong(TSC_ADC_STEPENABLE,
    (((1UL << (TP_FIFO_CNT * 2)) - 1) << 1) | /* Step Enable */
    (1 << 0)); /* charge step Enable */

    after

    am335xOutLong(TSC_ADC_CTRL, am335xInLong(TSC_ADC_CTRL) & (~1UL)); /* TSC Disable */
    while((am335xInLong(TSC_ADC_CTRL) & 0x00000001)); /* TSC Disable wait */

    am335xOutLong(TSC_ADC_IRQSTATUS, (1 << 5)); /* int clear*/
    am335xOutLong(TSC_ADC_STEPENABLE,
    (((1UL << (TP_FIFO_CNT * 2)) - 1) << 1) | /* Step Enable */
    (1 << 0)); /* charge step Enable */
    sysUsleep(1000); /* 1000 usec wait */
    am335xOutLong(TSC_ADC_CTRL, am335xInLong(TSC_ADC_CTRL) | 1UL ); /* TSC Enable */

    --------------------------------------------------------------------------------------

    It was necessary to wait after STEPENABLE was set up, but how long does it have to wait?

    Does it become FSM_BUSY if TSC_ADC is enabled after setting STEPENABLE without detecting the above wait processing or END_OF_SHEQUENCE?
    In that case, please tell me why it becomes FSM_BUSY.

    Best Regards,
    Shigehiro Tsuda

  • The factory team have been notified. They will respond here.
  • An unexpected event must have caused the Touch Screen/ADC state machine to enter an invalid state if it hangs.

    There is no way to guarantee every hang will have the same result.  There may be cases where a sequence like the one mentioned does something that allows the state machine to recover, but there may be others that will not respond to the sequence.

    The only way to guaranteed it recovers from a hung state is to reset the state machine. The only way to reset the state machine is applying power on reset to the device.

     

    Regards,

    Paul

  • Hi Paul,

    Thank you quick reply.
    I understand that FSM busy recovery is only power on reset.

    But Our customer seems to be returning in the following sequence after ADC hang by FSM busy.

    ① Set the enable bit of the CTRL register to 0.
    ② Resetting the STEPENABLE register
    ③ Set the enable bit of the CTRL register to 1.

    Will you check with your design team again?
    Recovery with POR reset can not be accepted as it can not be established as their product.

    Best Regards,
    Shigehiro Tsuda

  • The state machine was designed such that is does not have invalid states. If it hangs, something very bad happened and caused it to enter an invalid state. You may ask, how can a state machine enter an invalid state if it doesn’t have any invalid states. I will try to describe one such example.

     

    As you may know, a state machine transitions from one state to the next state based on various conditions which are evaluated at periodic intervals synchronous to the clock. The logic circuits within the state machine were designed to provide enough time for all conditions from the previous state to settle before being evaluating for the next state. This is known as timing closure and is based a maximum operating frequency for the clock. Setup/hold times to internal state machine flip flops may be violated if noise couples into the clock creating a glitch shortly before or after the real clock. This over-clocks the state machine by not providing enough time for the conditions from the previous state to propagate to the next state. The state machine may do very unpredictable things when this happens. In some cases the glitch may be very short and only propagate to a portion of the state machine flip flops. If either of these events occur, the state machine may enter an invalid state. This invalid state may resolve itself on the next state change, but there is no way to know for sure. Resetting the state machine is the only way to guarantee it recovers from this type of catastrophic event.

     

    Regards,

    Paul

  • I'm guessing the waveforms and hex dump of the FSM busy hang is posted here?

    I wonder if you are getting a FIFO overrun or underflow. From the AM335x TRM, Section 12.3.5:

    The FIFO can also generate FIFOx_OVERRUN and FIFOx_UNDERFLOW interrupts. The user can mask
    these events by programming the IRQENABLE_CLR register. To clear a FIFO underflow or FIFO overrun
    interrupt, the user should write a ‘1’ to the status bit in the IRQSTS register. The TSC_ADC_SS does not
    recover from these conditions automatically. Therefore, the software will need to disable and then again
    enable the TSC_ADC_SS. Before the user can turn the module back on, the user must read the
    ADCSTAT register to check if the status of the ADC FSM is idle and the current step is the idle step.

    You'd want to test that theory by enabling the IRQ ENable SET bits for FIFO1 overrun and underflow, and FIFO0 overrun and overflow.

    Regards, 

    Nick

  • Hi Paul,

    Thank you for quick reply.

    I understood as follows.
    If FSM busy occurs and TSC_ADC hangs, such software can be avoided in some cases, but in some cases it can not be avoided.
    Since these conditions can not be determined,there is only POR as a method to recover from FSM busy.
    Is it correct in my understanding?

    Best Regards,
    Shigehiro Tsuda

  • Hi Nick,

    Thank you for quick reply.

    [your question]
    I'm guessing the waveforms and hex dump of the FSM busy hang is posted here?

    [answer]
    Yes,register dumps and waveforms are those posted here.

    I will check what will happen if they enable FIFO overrun and underflow interrupts.
    Are there the sample programs?

    Best Regards,
    Shigehiro Tsuda
  • I do not know of sample programs using FIFO overrun and underflow interrupts. however, I would expect the user to set the IRQENABLE_SET bits for FIFO1 overrun, FIFO1 underflow, FIFO0 overrun, and FIFO0 overflow. After the FSM busy hang occurs, I'd look to see if any of those bits are set in IRQSTATUS register.

    Regards,
    Nick
  • Hi Nick,

    Thank you for various support.
    I checked the customer for FIFO overrun and FIFO underflow interrupt enable.
    As a result, this interrupt did not occur and the TSC ADC hung.

    Best Regards,
    Shigehiro Tsuda

  • Hello,

    Ok. Brad brought up another potential software cause for a TSC ADC hang in this post, could you check if the customer is doing something like polling for ADCSTAT[STEP_ID] == IDLE before writing to STEPENABLE? If not, it would be good to add that code and see if the hangs persist.

    Regards, 

    Nick

  • Hi Nick,

    Thank you for various support.
    There is no such processing in customer code.
    I will confirm with the customer what happens when ADCSTAT [STEP_ID] = IDLE polling processing is added before writing STEPENABLE.

    Best Regards,
    Shigehiro Tsuda
  • For future readers of this thread: Check out Brad's related comments on this post

    Regards, 

    Nick

  • Hi Nick,

    Thank you for various support.
    I confirmed Brad's comments on other post.

    Our customer seems to be able to recover after TSC ADC hangs in these sequences.
    It is confirmed that the frequency of occurrence varies depending on CPU load.
    Therefore, we think that the cause of TSC ADC hang is probably not a hardware factor such as noise.
    Is there no cause for hanging with software factors?
    I think that the state machine is hanging because there is timing that STEPENABLE can not write, since it is writing at that time.

    Best Regards,
    Shigehiro Tsuda
  • Hello,

    Did the hangs continue occurring after the customer added code that polls for ADCSTAT[STEP_ID] == IDLE before writing to STEPENABLE as per Brad's post? That is one software factor that could cause hangs if there is not a FIFO underflow/overrun.

    Regards, 

    Nick

  • Hi Nick,

    Thank you for your support.
    Updated additional information to the following post, please check.
    e2e.ti.com/.../2561646

    Sorry for delay.
    As for the result of Brad's proposed code addition, I am checking with the customer, please wait for a moment.

    Best Regards,
    Shigehiro Tsuda