This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2902C: signal lost in android environment

Part Number: PCM2902C
Other Parts Discussed in Thread: PCM2902

I have a question regarding the PCM2902C.

We are trying to receive stereo signals by inputting two analog signals using PCM2902C IC.

Two signals are recorded properly when the designed circuit is plugged into a USB in a PC window10 environment.

However, in the case of tablet devices (Glaxy tab 6, Android), only one signal is output even if two input signals are provided.

There must be a way to solve this.

Do you have to adjust the alternative settings that control the output by adjusting the interface so that the tablet also outputs two signals?

Maybe you know how to use alternative settings?

Please information.