Part Number: PCM1865
We have an issue where the PCM1865 on our PCA is not booting up correctly a small percentage of the time. Symptomatically the decimation filters do not appear to be configured correctly, such that low frequencies (~1khz) are represented correctly in the output data, while higher frequencies (~20khz) have significant attenuation.
PCM1865 configuration:
Sample rate: 96ksps
Output format: I2S with 2 DOUT pins for 4 channel output
Bus details: I2S master. BCK, LRCK both driven by ADC
Input clock: 38.4MHz high quality oscillator connected to SCKI
I recorded the I2C programming sequence on my oscilloscope with serial data logging, here is the sequence with timestamps and notes:
| Time | Address | Data | Notes |
| -43.04us | 4BW | 00 FE | reset |
| 34.16us | 4BW | 00 00 | page=0 |
| 111.3us | 4BW | 70 71 | pwr=standby |
| 188.3us | 4BW | 0B 00 | fmt=i2s |
| 265.4us | 4BW | 0C 00 | tdm=2ch |
| 342.4us | 4BW | 20 10 | clk=mstr, src=sck |
| 419.4us | 4BW | 21 01 | dsp1_clk=38.4M/2 |
| 496.5us | 4BW | 22 03 | dsp2_clk=38.4M/4 |
| 573.5us | 4BW | 23 0F | adc_clk=38.4M/16 |
| 650.5us | 4BW | 25 03 | sck_div=38.4M/4 |
| 727.6us | 4BW | 26 03 | bck_clk=38.4M/4 |
| 804.6us | 4BW | 27 3F | lr_clk=bck/64 |
| 881.6us | 4BW | 28 00 | disable PLL |
| 958.6us | 4BW | 29 01 | PLL P=1/2 |
| 1.036ms | 4BW | 2A 00 | PLL R=1 |
| 1.113ms | 4BW | 2B 05 | PLL J=5 |
| 1.190ms | 4BW | 2C B0 | PLL D = 0.12 |
| 1.267ms | 4BW | 2D 04 | PLL D = 0.12 |
| 1.344ms | 4BW | 28 01 | enable PLL |
| 1.421ms | 4BW | 70 72 | pwr=sleep |
| 1.498ms | 4BW | 11 50 | gpio3=dout2 |
| 1.575ms | 4BW | 71 30 | DSP: HPF en, IIR en |
| 1.652ms | 4BW | 06 50 | mux adc1L=1diff |
| 1.729ms | 4BW | 07 50 | mux adc1R=2diff |
| 1.806ms | 4BW | 08 60 | mux adc2L=4diff |
| 1.883ms | 4BW | 09 60 | mux adc2R=3diff |
| 1.960ms | 4BW | 01 28 | adc1L gain=20dB |
| 2.037ms | 4BW | 02 28 | adc1R gain=20dB |
| 2.115ms | 4BW | 03 00 | adc2L gain=0dB |
| 2.192ms | 4BW | 04 00 | adc2R gain=0dB |
| 2.269ms | 4BW | 00 00 | page=0 |
| 2.346ms | 4BW | 20 3E | clk=mstr, src=pll (98.304M). Dsp1_clk=pll_clk/2, dsp2_clk=pll_clk/4, adc_clk=pll_clk/16, bck=pll_clk/16 |
| 2.423ms | 4BW | 70 70 | pwr=run |
Afterwards, an I2C readback of all registers has 1 of 2 possible results. For a successful boot (majority of the time):
Page 0, Reg 0x01: 0x28
Page 0, Reg 0x02: 0x28
Page 0, Reg 0x03: 0x00
Page 0, Reg 0x04: 0x00
Page 0, Reg 0x05: 0x86
Page 0, Reg 0x06: 0x50
Page 0, Reg 0x07: 0x50
Page 0, Reg 0x08: 0x60
Page 0, Reg 0x09: 0x60
Page 0, Reg 0x0a: 0x00
Page 0, Reg 0x0b: 0x00
Page 0, Reg 0x0c: 0x00
Page 0, Reg 0x0d: 0x00
Page 0, Reg 0x0e: 0x00
Page 0, Reg 0x0f: 0x28
Page 0, Reg 0x10: 0x01
Page 0, Reg 0x11: 0x50
Page 0, Reg 0x12: 0x00
Page 0, Reg 0x13: 0x00
Page 0, Reg 0x14: 0x00
Page 0, Reg 0x15: 0x00
Page 0, Reg 0x16: 0x28
Page 0, Reg 0x17: 0x00
Page 0, Reg 0x18: 0x00
Page 0, Reg 0x19: 0x00
Page 0, Reg 0x1a: 0x00
Page 0, Reg 0x1b: 0x00
Page 0, Reg 0x20: 0x3e
Page 0, Reg 0x21: 0x01
Page 0, Reg 0x22: 0x03
Page 0, Reg 0x23: 0x0f
Page 0, Reg 0x25: 0x03
Page 0, Reg 0x26: 0x03
Page 0, Reg 0x27: 0x3f
Page 0, Reg 0x28: 0x01
Page 0, Reg 0x29: 0x01
Page 0, Reg 0x2a: 0x00
Page 0, Reg 0x2b: 0x05
Page 0, Reg 0x2c: 0xb0
Page 0, Reg 0x2d: 0x04
Page 0, Reg 0x30: 0x00
Page 0, Reg 0x31: 0x00
Page 0, Reg 0x32: 0x00
Page 0, Reg 0x33: 0x01
Page 0, Reg 0x34: 0x00
Page 0, Reg 0x36: 0x01
Page 0, Reg 0x40: 0x80
Page 0, Reg 0x41: 0x7f
Page 0, Reg 0x42: 0x00
Page 0, Reg 0x43: 0x80
Page 0, Reg 0x44: 0x7f
Page 0, Reg 0x45: 0x00
Page 0, Reg 0x46: 0x80
Page 0, Reg 0x47: 0x7f
Page 0, Reg 0x48: 0x00
Page 0, Reg 0x49: 0x80
Page 0, Reg 0x4a: 0x7f
Page 0, Reg 0x4b: 0x00
Page 0, Reg 0x4c: 0x80
Page 0, Reg 0x4d: 0x7f
Page 0, Reg 0x4e: 0x00
Page 0, Reg 0x4f: 0x80
Page 0, Reg 0x50: 0x7f
Page 0, Reg 0x51: 0x00
Page 0, Reg 0x52: 0x80
Page 0, Reg 0x53: 0x7f
Page 0, Reg 0x54: 0x00
Page 0, Reg 0x55: 0x80
Page 0, Reg 0x56: 0x7f
Page 0, Reg 0x57: 0x00
Page 0, Reg 0x58: 0x00
Page 0, Reg 0x59: 0x00
Page 0, Reg 0x5a: 0x00
Page 0, Reg 0x60: 0x01
Page 0, Reg 0x61: 0x00
Page 0, Reg 0x62: 0x10
Page 0, Reg 0x70: 0x70
Page 0, Reg 0x71: 0x30
Page 0, Reg 0x72: 0x0f
Page 0, Reg 0x73: 0x04
Page 0, Reg 0x74: 0x32
Page 0, Reg 0x75: 0x00
Page 0, Reg 0x78: 0x07
Page 1, Reg 0x01: 0x00
Page 1, Reg 0x02: 0x00
Page 1, Reg 0x04: 0x00
Page 1, Reg 0x05: 0x00
Page 1, Reg 0x06: 0x00
Page 1, Reg 0x07: 0x00
Page 1, Reg 0x08: 0x00
Page 1, Reg 0x09: 0x00
Page 1, Reg 0x0a: 0x00
Page 1, Reg 0x0b: 0x00
Page 3, Reg 0x12: 0x40
Page 3, Reg 0x15: 0x01
Page 253, Reg 0x14: 0x00
For a flawed boot (minority of the time), the only difference was that register 0x14 read 0x08 and register 0x73 read 0x03. This incorrectly detected sample rate seems to match the symptom of the incorrectly set up decimation filter. Not sure if there is anything we are doing wrong? One other observation is that the PLL lock bit in register 0x28 never seems to go high. Is that a known issue or a problem with our configuration?
Any suggestions?
Thanks!
Tim Burnett