Part Number: PCM1865
Hello,
I'm having a hard time getting PLL to lock,
the MCLK source for PCM1865 is a 12MHz 50ppm oscillator, then configuring PLL I do see the expected frequencies on SCK/BCK/LRCK pins, but no lock (reg 0x28 b4)
Config for Fs 48000:
pll: k = 8.1920 p=1 r=1, dsp1: 4, dsp2: 8, adc: 16, sck: 8, bck: 4, lrck: 64
Full registry dump:
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: 00 00 00 00 00 86 41 41 42 42 00 4c 00 00 00 00
10: 30 52 44 40 00 f0 00 00 00 00 00 00 00 00 00 00
20: 7e 03 07 0f 50 07 03 3f 01 00 00 08 80 07 00 00
30: 00 00 00 01 00 00 01 00 00 00 00 00 00 00 00 00
40: 80 7f 00 80 7f 00 80 7f 00 80 7f 00 80 7f 00 80
50: 7f 00 80 7f 00 80 7f 00 00 00 00 00 00 00 00 00
60: 01 00 10 00 00 00 00 00 00 00 00 00 00 00 00 00
70: 70 10 0f 03 32 00 11 c4 07 00 00 00 00 00 00 00
80: 00 00 00 00 00 86 41 41 42 42 00 4c 00 00 00 00
90: 30 52 44 40 08 f0 00 00 00 00 00 00 00 00 00 00
a0: 7e 03 07 0f 50 07 03 3f 01 00 00 08 80 07 00 00
b0: 00 00 00 01 00 00 01 00 00 00 00 00 00 00 00 00
c0: 80 7f 00 80 7f 00 80 7f 00 80 7f 00 80 7f 00 80
d0: 7f 00 80 7f 00 80 7f 00 00 00 00 00 00 00 00 00
e0: 01 00 10 00 00 00 00 00 00 00 00 00 00 00 00 00
f0: 70 10 0f 03 32 00 11 c4 07 00 00 00 00 00 00 00
There were similar problems discussed in this forum previously, but in my case, PLL wont lock even with config sequences provided there (values adjusted for 12MHz clock):
i2cset -y -f 1 0x4a 0x00 0xFE i2cset -y -f 1 0x4a 0x00 0x0 i2cset -y -f 1 0x4a 0x25 0x7 i2cset -y -f 1 0x4a 0x26 0x3 i2cset -y -f 1 0x4a 0x27 0x3F i2cset -y -f 1 0x4a 0x20 0x7E i2cset -y -f 1 0x4a 0x28 0x01 i2cset -y -f 1 0x4a 0x21 0x03 i2cset -y -f 1 0x4a 0x22 0x07 i2cset -y -f 1 0x4a 0x23 0x0F i2cset -y -f 1 0x4a 0x29 0x00 i2cset -y -f 1 0x4a 0x2a 0x00 i2cset -y -f 1 0x4a 0x2b 0x08 i2cset -y -f 1 0x4a 0x2c 0x80 i2cset -y -f 1 0x4a 0x2d 0x07
Am I missing something?
Also, is there any ETA for the new revision of datasheet?