Hello, we are using the PCM1865A configured in a four single ended inputs mode for microphone acquisition.
We noticed a noise problem and in the search for it, we basically removed all the front end components (only passive), ending with the PCM1865 input connected to the GND plane. The noise is still present. See images in the attached file.
Then we connect the input to the PCM1865 REF pin and the noise disappears. See last image in the attached file.
We are quite puzzled by this results as it would indicate a device internal noise source that is nullified when acquiring VREF rather than GND, while the actual measure is (IN - VREF) as shown by the device MUX function in its datasheet. On in other words that noise source is present on the VREF input.
We tried some changes around the PCM1865 power supply (tie to an external linear lab PSU), decoupling (VREF and power supply) without any succeess.
Does somebody have a suggestion about the possible noise source given the above experiment result ?
Best regards