This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirs,
Would you please provide the specification of PSRR (power supply rejection ratio) in dB of the OPA1632?
We see the specification of input offset voltage vs power supply only in the OPA1632 datasheet only.
Thank you and Best regards,
Wayne Chen
07/09/2021
Hello Wayne,
We do have PSRR for the OPA1632 which is not in this datasheet. The PSRR for load of 800Ohms, Vs +/-5V is 73dB min and 98dB typical at ambient temperature. For full range temperature, PSRR is 70dB minimum. Here is also a plot of PSRR vs Frequency.
Thank you,
Sima