Part Number: TAS5805M
We have TAS5805M designed with PBTL configuration for subwoofer operation.
The TAS5805M has PVDD=22V, output using L = 10uH and C=1uF, BD mode, Fsw = 768KHz, BW = 80KHz, LPF -3dB cutoff = 75Hz, output limit to <35W.
We noticed that when we sweep a 0dB 50~100Hz signal, at 75Hz, the TAS5805M will cutoff the output and issue OCP error.
The speaker impedance is about 31ohm at 75Hz, with a phase shift from -53deg to 53deg.
After we adjust AGL, we are able to suppress the OCP.
We managed to measure that with 75Hz at maximum output, the peak current is about 1A. This is way below the 5A OCP limit.
How can OCP be triggered?
We also noticed that adjusting AGL threshold is able to prevent the OCP and lower the peak current (measured at PVDD) at the same time.
Is OCP actually triggered by the suge current due to internal MOSFET switching?