This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM4220: Maximum operating junction temperature

Part Number: PCM4220
Other Parts Discussed in Thread: PCM4222

What is the maximum thermal junction operating temperature for this component? 

  • Also, the same information is needed for PCM4222.

  • Hello,

    I believe it is this spec that i have highlighted that you are looking for:

    It is same for 4222.

    Best,

    Carson

  • Is this representative of the maximum component junction temperature (temperature at the core of the component)? I was under the impression the 85°C temp is an ambient outside air temperature. 

  • Hello David,

    Yes you are correct about that, that was my mistake. What exactly is the application of this part to be worried about junction temperature?

    As long as you are within ambient range junction temperature should not be a problem since this is not a high power dissipating part.

    Based on other Audio ADCs the junction temperature would actually be closer to the storage temperature max but I cannot guarantee that nor do I easy way of getting the junction temperature for this specific part.