Other Parts Discussed in Thread: TAS2557
Hi Sirs,
We have met some problems on TAS2557EVM operation.
We used it normally the day before, but we today we turned on the power for TAS2557EVM board, the PPC3 can’t connect to device.
Here are the steps we checked.
- We checked all of the power are good(5V,3.3V, 1.8V), and the power current is also normal.
- It is not short or broken.
- We could measure 6MHz on the Y1 output pin.
- The USB path connecting from laptop side to MCU side is good.
- Reinstall PPC3 tool and TI USB driver from laptop and other computer.
Base on above steps, the connecting is still broken.
- We checked the I2C signal then we found it showed A0/A1 data is 25 only.
It didn't have other information when we power on device.
And then we check the jumper, we found that it didn't connect J24(WP) jumper on default when we got the EVM. But the user guide line showed that it should be inserted on default.
The result should be that the EEPROM may have been re-flashed for unknown state.
Do you have any solution can help us?