Part Number: PCM1754
Hello,
Our customer applies Reset when input PCM data Fs is changed. Because in this sequence, sometime PCM1754 is made degradation of SNR issue, and it was solved by Reset.
Here is question, PCM1754 Power On Reset condition is Vcc>2.2Vmin as datasheet is described.
However in our experiment, it seems there is one more condition which is Vcom voltage also needs to less than 2.2V to assert internal POR.
Otherwise low SNR situation is not cleared. So actual device behavior shows somehow monitor Vcom and Vcc for POR.
As our countermeasure, we will apply long enough Vcc power down period to reach less than 2.2V Vcom.
Can you expect such internal connection path POR circuit to Vcom and our design approach is acceptable?
Regards,
Mochizuki