This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use TLV320AIC3253EVM-K. My trouble is that we cannot DL our Program to TLV320AIC3253EVM-K.
I try below
1,Create a sample circuit --- OK (Yes. I can find TLV320AIC3253)
2,Build -> Genarate Code --- OK
3,Build -> DownLoad and Run ---NG
4,Tools -> I2C memory tool -> Setup -> Board FWID
I cannot find TLV320AIC3253EVM. So We download FW to TLV320AIC3253EVM
How do I resolve?
<sample circuit>
<Memory Tool menu> We cannot find TLV320AIC3253EVM-K.
<Log>
Generating code for base_main_Rate48 .. assembling .....Done.
Build succeeded.
Found board type: FWIDTLV320AIC3254EVM-K.
Warning: The FWID of the board, FWIDTLV320AIC3254EVM-K, does not match the framework in the Process flow.
Board sampling rate: 48000Hz.
Downloading base_main_Rate48.cfg to the EVM.
done.
<Version>
Hi,
For trouble downloading image to AIC3254EVM I suggest following the step-by-step instructions outlined in GDEQuickStartGuide073010.pdf (1.4.2)
More information can be found in GDEUserGuide060710.pdf