This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Selecting an amplifier with audio compression

Hi,

I am looking for a sound amplifier with a sound compression.
For applications with better talk sound to headset or speaker (about 2W).
Ideally, reduce high volume sound (loud speech, shout, gunshot) and amplify low volume sound (low speach, whisper).
No need for great sound quality. It will be powered by a small battery.

Hard requirements:
Power voltage 3.3V or 5V or similary.
Audio compression
Low price
Low size

Soft requirements:
Setting volume over i2c or any
Stereo output Class-G or Class-D
Noise suppression