This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Expert
Follow the power sequence comment from below
If our design AVDD&DRVDD(3.3V) is powered on before IOVDD & DVDD (with same 1.8V source) will also cause leakage current?
Regards,
Vincnet
Hi Vincent,
I don't have data showing a leakage current, but I would say yes that it would cause leakage current. The AIC3107 is very robust and the power sequencing can be quite flexible, so there isn't necessarily any problem or risk of damage with applying AVDD/DRVDD before IOVDD/DVDD. But if through testing you find the leakage is a concern, I would advise following the recommended sequence.
Best regards,
Jeff McPherson