This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In the design, the MCLK is not used. So, how the MCLK pin is connected?
Can it be connected to the ground or floating?
Can it be connected to the Capacitance to ground as shown in the picture?
Thank you so much!
Hi Leo
The datasheet sates there's internal clock, could be used during MCLK missing. But sadly there's too little information about it, and I can't be sure if all the function could be supported on this internal clock.
So I strongly suggested give a suitable MCLK for your using, choosing according to below table.