Other Parts Discussed in Thread: TLV320DAC3203
Hi Ivan,
going on with the settings of the TLV320DAC3203, I am now testing with a higher MCLK.
I read in the Reference Guide (slau434a), by the settings for Fast Startup:
"The system used to develop this configuration has a MCLK input of 12.288-MHz, the device is configured as slave for the I2S interface and the sampling frequency is 48-kHz. So the device would only need to divide MCLK by 256 to obtain the desired sampling frequency, thus there is no need to power up and configure the PLL. As a side note, keep in mind that it is always recommended to set DOSR to 128 for best audio quality"
So, actually, the PLL is not being used by this MCLK frequency.
Since I cannot find how to change the frequency of MCLK in the EVAL Kit, I decided to try with the standard frequency of 11.296-MHz
With this MCLK being divided by 256, we get 44.1 kHz Sampling frequency. Here too, the PLL should not be needed.
However, the EVM powers the PLL on.(Digital Microphone Loopback Script)
If I deactivate the PLL, the Mics are not geting any clock.
Any reason for this? What should I change in the script to avoid using the PLL (and save on energy consumption)?
Best regards from Germany!
Gustavo