Part Number: TLV320ADC3100
Other Parts Discussed in Thread: TLV320ADC3120
Hi,
We are using the TLV320ADC3100 audio codec for our project. We write in the register first, and then we verify it by reading the registers. However, the value we get after reading the register is different from what we wrote there. Is there anything we have to take care for I2C peripheral?
We have configured the Audio codec in master mode and our desire output is:
BCLK: 2.8224Mhz
WCLK: 44.1khz
Sample Size: 32-bit
For that we have given the MCLK of 12.288Mhz.
Also, below are the configured register's value.
ADC310X_PAGE_SELECT - 0x00 // Page - 0 selected
ADC310X_RESET - 0x01 // Soft Reset
ADC310X_CLK_GEN_MUX - 0x00 // Clock Generation
ADC310X_PLL_PR_VAL - 0x91 // PLL_CLK - 90.3168
ADC310X_PLL_J_VAL - 0x07 // J - 7
ADC310X_PLL_D_VAL_MSB - 0x0D //
ADC310X_PLL_D_VAL_LSB - 0xAC // Combination of MSB and LSB is 3500 for D
ADC310X_NADC_CLK - 0x88 // NADC - 8
ADC310X_MADC_CLK - 0x82 // MADC - 2 as per our calculations
ADC310X_AOSR - 0x80 // Oversampling - 128
ADC310X_ADC_IADC - 0x20 // IADC - 32
ADC310X_ADC_INTF_CTRL_1 - 0x3C // i2s for adc interface with 32 bits sample size, both BCLK and WCLK as output
ADC310X_ADC_INTF_CTRL_2 - 0x06 // BDIV_CLKIN = ADC_CLK and both are active even with the codec powered down
ADC310X_BLCK_N_DIV - 0x82 // Value is 2 as per our calculations.
ADC310X_ADC_PROC_BLK- 0x01 // ADC signal processing block PRB_R1
ADC310X_PAGE_SELECT - 0x01 // Page - 1 selected
ADC310X_PGA_ANALOG_L - 0x00 // Left PGA gain = 0 dB and muted
ADC310X_PGA_ANALOG_R - 0x00 // Right PGA gain = 0 dB and muted
ADC310X_INPUT_SEL_PGA_L_1 - 0xfc // Left ADC Input selection for Left PGA = IN1L(P) as Single-Ended
ADC310X_INPUT_SEL_PGA_R_1 - 0xfc // Right ADC Input selection for Right PGA = IN1R(M) as Single-Ended
ADC310X_PAGE_SELECT - 0x00 Page - 2 selected.
ADC310X_ADC_DIGITAL - 0xc2 // Power-up Left ADC and Right ADC
ADC310X_ADC_VOL_CTRL - 0x00 // Unmute digital volume control and set gain = 0 dB
Please suggest some suggestions.
Thanks & Regards
Lakshita

.