Other Parts Discussed in Thread: TPA2012D2
Hello,
I have developed a cellular device, and I need help to solve the handsfree volume level. The circuit consists of a Quectel EG91 module, a TLV320AIC3104 IC and a TPA2012D2 interconnected as follows:

where the audio block is,

* the RESET pin (31) has been corrected
* R43 and R44 are not fitted
The CODEC headphone outputs work correctly, and you hear at the proper volume. It turns out that I am unable to measure the RMS voltages on the TLV320AIC3104 outputs, so that I can compare them to the specs. As I understand, and as expected, is that through the lines of pins 27, 28, 29 and 30 I can observe values like the following:

I am able to measure on scope a signal in the order of 50mVpp which coincides with the frequency of the tone I am trying to reproduce.
I assume that the power amplifier (TPA2012D2) works well, since if a signal of approximately 500mVpp is injected in the inputs pins 16, 17, 19 and 20; the speakers reproduces the sound with the expected volume.
I have made modifications on the board to bring the circuit to the recommended ones:

and

But I still don't have more amplitude in the signals, and therefore volume.
The speaker selected is https://www.cuidevices.com/product/resource/cms-160925-078x-67.pdf
I appreciate the help in advance
Greetings,