Part Number: SRC4392
I have a current product with 4 CS8422 SRC , which is now obsolete. I am looking into replacing the all 4 CS8422 with the SRC 4192.
The current configuration is the product has 4 AES3 inputs and 4 AES outputs (CS8406) with the AES3 input sample rate ( 44.1 to 192k )converted either 48 or 96 khz.
It also has 8 analog ADCs and DACs. The ADC and Digitla inptus all feed 4 dsp chips.
The first CS8422 acts as the Master ( MCLK, BCLK LRCLK ) and all the other devices act as slaves including the IO so everything is synced.
So I what to duplicate the setup with 4 SRC4392. All the SRC4392 will be programmable thru I2S