Hi everyone, I hope someone can help me.
I had a Simaudio Andromeda CD player which uses 2 PCM1704-K DACs per channel.
One of these failed (one of the two 1704-k dedicated to Left channel) and had to be replaced.
The technician I turned to, installed a PCM1704 but without the K and the player works, I must say that I don't notice any differences, but I would like to know if it is a K version or not and the technician can't tell me unfortunately.
The two DACs work together on the left channel: is it possible that a K and a NON-K version can work together?
any comments, experiences or help are appreciated
Thank you