Part Number: PCM6260-Q1
Other Parts Discussed in Thread: INA121
Hi
Customers encountered new problems when using pcm6260. Two of them were related to channel gain adjustment and automatic gain controller.
1. Situation 1: When I fix CH1_CFG2 Register (Digital volume) = 241d = 20dB and only adjust CH1_CFG1 Register (channel gain), start from 0 and adjust upward. When it exceeds 7dB, channel 1 cannot receive sound.
2. In the second case, CH*_CFG2 Register (Digital volume)=241d=20dB is still fixed, and Channel * automatic gain controller (AGC) setting is used instead, enable When the 1khz sound is not provided, very loud noise will be received, or when the 1khz signal is deliberately interrupted for a short period of time, the unrecognizable noise will be obvious.
P.S. tdm-32b-hw0_0_ch1_0x3d_6db_*db.png is to adjust channel gain tdm-32b-hw0_0_ch_1_adc.png Five screenshots of AGC enabled, from ch1 to ch5. tdm-32b-hw0_1_ch_123_adc.png and tdm-32b-hw0_1_ch_12345_adc.png are the cases where AGC is enabled on the channel together.