This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3104EVM-K: No communication from AIC310x EVM GUI to the dev board via USB

Part Number: TLV320AIC3104EVM-K


Hi TI, I am trying to use the AIC310x EVM GUI.  When I select a Preset Configuration and press load, nothing happens.  If i click the Command Line Interface tab i see the 'bus error' indicator lit. In the Device Manager I have a error on the TI USB Audio 2.0 and when i look at the properties it states 'this device cannot start. (code 10)'  I am not positive these 2 things are related but it's my only clue at this time.  I was also, getting a Texas Instruments DFU error as well but i was able to find a driver for this and clear the error.