Part Number: INA1650
Other Parts Discussed in Thread: OPA1677, OPA1688
In the datasheet of OPA1677, there's an example circuit (copied below) that illustrates the use of said op-amp to force the output voltage of a INA1650 stage to 0v. However, the input to the INA1650 is AC-coupled, so there should not be any DC going through; shouldn't the voltage of A equal IN+A minus IN- A ? So maybe I'm missing a piece of the puzzle and I'd like to understand it before I finalize my circuit based on the INA1650.
Now I guess there could be a potential difference between the chassis ground and the circuit ground. If the COM inputs are tied to the chassis ground, as they are in this example via 1M ohm resistor, could that incur a DC offset, and that is what needs to be removed? I couldn't see much in the datasheet regards the COM inputs and I couldn't find the model in TINA for INA1650 to test that. If that is the case, I could just tie the COM pins to local ground instead, but perhaps that would adversely affect CMMR?