Part Number: TAS2780EVM
Other Parts Discussed in Thread: TAS2780, PUREPATHCONSOLE
Hello Audio Amp team,
I had a question regarding how to interpret the SDOUT data. My team is using the TAS2780EVM with PurepathConsole to configure the TAS2780EVM over I2C but have begun to stream audio data to the TAS2780EVM using an external development kit. My team also has the development kit set up to read back the SDOUT data. In Purepathconsole, the TAS2780 is configured for only the I-sense data now. Here is the PPC3 file we are using in the set up.
An initial test we removed the speaker from the output terminals expecting that the SDOUT would report 0A. Generally the readings we see are 0x0010 - 0x00F9 but we also get readings of 0xFF00. I wanted to confirm that a reading of 0x000 = 0A and 0xFFFF = 5A and that each LSB is about 77uA? Also what type of reading should we expect when we have the speaker disconnected?
Our current set up only allows us to read/record the first SDOUT measurement. Could we expect bad data on the first measurement and if we read the next few measurements we would see measurements close to 0A?
Thank you,
Kessler