This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TIer
Could you recommend a chip as next generation of TLV320DAC3100.
The customer needs an updated chip.
In a new project, the project manager requires production time to compare the new chip.
Hi,
Are you looking for a device with a 2.5W amplifier like the TLV320DAC3100? Unfortunately, we do not have any other DACs with amps that are this high power. You can check out the TLVAIC3100 which is a codec with the same amplifier, if you would like an ADC integrated into the device as well, or you could look into our amplifiers line to find an amp with a digital in. The TAS2505 and the TAS2521 are good options to look into. We have some DACs with 0.5W amplifiers. Unfortunately our newer line of converters do not have integrated amplifiers.
I hope this answers your question and let me know if you need more recommendations, if you have specific requirements for the project.
Best,
Mir