Part Number: PCM5100A
Other Parts Discussed in Thread: PCM1808, PCM5100
Tool/software:
Hi
Our product's audio block diagram is as follows
We use a PC to verify the basic functionality of the channels.
For the MIC channel, we listen to the device through the PC and then hear the sound through the SPEAKER.
During this test, we can hear noise in the MICROPHONE channel, and the noise increases with the MICROPHONE dB Level.
The MICROPHONE and SPEAKERuse PCM1808 for I2S audio A/D conversion, which transmitted to PCM5100 for D/A conversion and sent to the PC.
The design as follows: this is for the audio bypass function.
Questions:
- Have there been any similar noise issues encountered by other RD when they using PCM1808 with PCM5100 for the MICROPHONE channel?
Are there any countermeasures which can advice us?