Other Parts Discussed in Thread: PUREPATH-CMBEVM, PUREPATHCONSOLE
Tool/software:
Hi,
I am new to the TI smart amplifier ecosystem. We are trying to evaluate the TAS5825EVM and have also bought the PUREPATH-CMBEVM Motherboard
We have installed the PurePath Console v3.2.1 in our windows 10 PC
Installed the EVM GUI SW -TAS5825M GUI for PurePathConsole 3
Connected the Motherboard to the PC
Applied external 5V to PVDD on the EVM daughter board
Connection is succesful but I am not able to do the system check - hardware check always fails and says download unsuccesful. We only have one PurePath Motherboard and one TAS5825 eval board

The Motherboard is detected by the PC and below are the details of the windows driver that is in use.

Driver Name: wdma_usb.inf
Class Guid: {4d36e96c-e325-11ce-bfc1-08002be10318}
Driver Date: 04/12/2024
Driver Version: 10.0.19041.4355
Driver Provider: Microsoft
Driver Section: USBAudio
Driver Rank: 0xFF2002
Matching Device Id: USB\Class_01
Outranked Drivers:
Device Updated: false
Parent Device: USB\VID_0451&PID_BB02\6&26ef9c29&0&1
Hardware Setup

I also tried connecting a small speaker and playing an audio in the PC - there is no output sound
Kindly Help
Thanks