Other Parts Discussed in Thread: AM5728, TLV320AIC3212,
Tool/software:
Hello,
We had done the following trail, as suggested in the previous query :
The ADC Channel Volume Control (B0_P0_R84/83) register value has been adjusted upward (tuned), and the AGC register (B0_P0_R88) value has been lowered (tuned) as suggested.
Increasing or decreasing the value of the B0_P0_R84/83 register shows no noticeable impact on volume. Additionally, reducing the AGC value has decreased mic pickup, which is affecting normal call conversations. Current AGC (B0_P0_R88) Value 36db.
However, changes to the B0_P0_R84/83 register value do not affect the loudness of the volume.
We had attached the scripts to set register values for handsfree mode in previous post.
Please suggest a way to tune AGC parameter values, to reduce noise capture. We are also facing issue of shrill at higher volumes and echo when user switches between handset and handsfree mode.