Other Parts Discussed in Thread: TLV320AIC3120
Tool/software:
I am working with TLV320AIC3120 EVM. I am using codec control software to configure the codec, so as to test the ADC and DAC. I have taken the default log which comes once I connect the EVM to my system. I made the same log to be executed in the EVM. I have connected mic and speaker in the two jacks provided and have tested and verified that mic and speaker is working. The default sampling frequency is 44.1 KHz. Now, I want to change the sampling frequency to 8 KHz. I have tried changing it thorugh codec control software, so as to get automatic log accordingly. But I could'nt do it. Is there any way by which I can do it? Finally, I want to interface the board with the PSOC6 microcontroller eval board, so that I can program the codec through I2C registers. My requirement is 29.4912 MHz master clock from an external oscillator and 8 KHz sampling frequency. I want the corresponding log for this, so as to program codec with microcontroller.