Tool/software:
Hi Team,
I have used DRV135 to convert single-ended to differential signal.
There is a noticeable difference between the P and N output values of the DRV135. Can anyone help determine the exact cause?

Below are the observations:
Vin: 3V
Across P & N = 6.45V
P v/s GND = 3.25V
N v/s GND = -3.18V
Vocm = 250mV(max) // As per datasheet
Vodm = 10mV(max) // As per datasheet