Part Number: DRV135
I am currently using DRV135UA from TI in my design. I am using it as single ended to differential conversion circuit. Power supply for the IC is +15V,-15V with 1uF capacitor on both rails. VO+ is connected to -SENSE via 10uF cap and VO- to -SENSE via 10uF cap. My input voltage range w.r.t GND is -5V to 5V. So as per datasheet i should get 10V for 5V input and -10V for -5V input, across VO+ and VO-. But my observed readings are given below.
| Input | Output |
| 5 | 23.050 |
| -5 | -23.040 |
then i shorted the both 10uF caps with 0 ohms resistors. then i am getting this
| Input | Output |
| 5 | 10.850 |
| -5 | -10.830 |
then i tried putting a load of 1.105K ohms resistor between VO+ and VO-, voltage reduced to
| Input | Output |
| 5 | 10.340 |
| -5 | -10.320 |
Again i increased load to 660 Ohms then voltage reading again reduced to
| Input | Output |
| 5 | 10.060 |
| -5 | -10.040 |
So in order to get a gain of exact 6dB what should i do?? as per datasheet there is no minimum load requirement to get the specified gain