Tool/software:
I found this forum post from a while ago, where this user had a very similar problem that I am having with the PCM2912A:
The audio playback and microphone recordings sound clear and fine, except that during audio playback there is a ~300BPM rapid ticking sound, and during microphone recordings there is a repeating audio buzz, about every 0.8 seconds.
My schematic for reference, I believe is 1 to 1 with the recommended schematic in the datasheet, though I have added a headphone detection circuit to it:
I've attached an MP3 file showing the sound oddities.
The first 8 seconds is the chip recording a 300Hz sine wave via a headset microphone (I held a speaker up to the mic that was playing the tone). You can hear a sharp buzz every 0.8 seconds or so.
The next 8 seconds is recording the audio output of the chip into my audio interface. Same 300Hz sine wave being played, and you can hear there is a ~320BPM ticking sound.
For reference I've tried using the board with my computer, changing the sample rate and bit depth had no effect. The final application for this board will be using it with a USB-C iPad, and I have the same problem when connecting it to an iPad.
Anyone have an idea for what the problem could be?
Thanks,
Matt