This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I'm using PCM1861-Q1 ADC with H/W conrol mode and I2S format by connection 12.288MHz OSC as below to make a default 48KHz Fs rather than 24.576MHz Crystal. It's located close enough to IC
But sometimes, there is not working situation so when putting a few pF(18pF) to C22, C25 without crystal, this situation has been disappeared..
Previously, I used 24.576MHz crystal with this 18pF and I never encoutered this one..
In PCM1861-Q1, is it having some weak point when using 12.288MHz OSC? If so, is it OK to put a few pF like above without crystal? Help to get your advice
By the way, I'm using also PCM1821-Q1 together with putting 12.288MHz OSC but in PCM1821, it's working well without such an issue.
Help to get your supporting to identify it
Thanks
Best regards,
Jaydon
Closing because duplicate thread, please follow response here: https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1448062/pcm1861-q1-pcm1861-q1-adc-oscilator-or-cyrstal-usage