Part Number: LM4871
Tool/software:
I built up the circuit of LM4871M just as typical circuit shown, but the output of LM4871M would always be 5V. How could I solve it?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM4871
Tool/software:
I built up the circuit of LM4871M just as typical circuit shown, but the output of LM4871M would always be 5V. How could I solve it?


Hi Meihan,
Our support on simulation models is limited, but I'll add a few comments below:
Besst regards,
-Ivan Salazar
Applications Engineer
Hi Ivan,
Thank you for your reply. I found that if I swap the input pins then the circuit work fine.

It's really strange because now the two pins connections are opposite to the datasheet.
Kind regards,
Meihan
Meihan,
This may be due to how the model has been described. Unfortunately, there is no EVM available for this device, but a simple PCB could be built to test the actual device.
Best regards,
-Ivan Salazar
Applications Engineer