Other Parts Discussed in Thread: TAA5212, TAS6584Q1EVM
Tool/software:
Could not connect via USB to TAA5212EVM-K on PPC3. (windows11)
The lower left corner of the screen is fixed showing TAA5212 - OFFLINE.
Device manager shows TI USB Audio UAC2.0 and the connection between windows and TAA5212EVM-K appears to be working.
Another PC (windows 10) confirmed the connection.
Although the devices are different, the symptoms may be similar to the following condition.
TAS6584Q1EVM: PurePath Console 3 v3.2.1 Build 306 & TAS6584 3.03 cannot connect to EVM through USB (Windows 11)
https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1224017/tas6584q1evm-purepath-console-3-v3-2-1-build-306-tas6584-3-03-cannot-connect-to-evm-through-usb-windows-11
Can you suggest a way to solve this problem?
Best regards.