This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3156D2: Control the SDZ and MUTE pins with 3.3V logic levels

Part Number: TPA3156D2


Tool/software:

Hello, everyone.
I can't find any information anywhere. Can I control the SDZ and MUTE pins with 3.3V logic levels directly from the microcontroller? Or are all levels tied to PVCC?

  • Hi Ihor,

    You could use 3.3V logic to control the SDZ and MUTE pins. In the datasheet, it is specified that the high-level input voltage for MUTE and SDZ is 2V and the low-level input voltage is 0.8V.

    Regards,

    Ramsey

  • I'm just confused by other discussions in the forums. Yes, the datasheet seems to be clear, but the line “TTL logic levels with compliance to AVCC.” was confusing, since my AVCC is 24 volts. In the end I tested it in practice and it works. Thanks for your reply.