Part Number: PCM5102A
Tool/software:
Hi team
Is there a table showing the LOUT output voltage for 24-bit audiodata?
I will be using an audio data word = 24-bit, BCK =64fS, so I will use the method where all bits after the LSB are 0.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM5102A
Tool/software:
Hi team
Is there a table showing the LOUT output voltage for 24-bit audiodata?
I will be using an audio data word = 24-bit, BCK =64fS, so I will use the method where all bits after the LSB are 0.
Hello,
There is no table showing the LOUT voltage as you have noticed in the datasheet, and I don't recall I have seen this kind of table before. All the information regarding this IC, including any existing applications notes , can be found in the product page.
Regards,
Arash
Sure, this is the first page of the IC documents in ti.com. So it is
https://www.ti.com/product/PCM5102A
Sometimes you can find useful docs or application notes on similar IC' s product page as well.
Regards,
Arash
I have checked this link. Even after checking it, I could not find any information that explains the relationship between the output voltage and audio data, so I am asking. Please let me know of a document or a link that explains the relationship between the output voltage and audio data.
Hello, as I mentioned above, IF there is any additional document related to the device , it can be found on the product page. This is true for any product. All available documents could be found in its product page.
I don't recall I have seen a table for Vout vs. input data/code in any datasheet. But you can calculate the output , for example lets say all ONEs will give full scale of 2V at the output , and all Zeros will give 0V, similarly a mid code ( i.e, 100000....00000 ) will give the mid scale , so you can roughly calculate it based on LSB and code and reference voltage.
Regards,
Arash
This product has an output of 2.1VRMS centered around GND, so I understand it can be set from -2.9V to +2.9V.
Is it correct that the output for "0x000000" is 0V? Is the maximum setting for positive output "0x7FFFFF"? Or is it "0xFFFFFF"?
Also, is it correct to understand that when "0x000001" is set, the voltage is 0.35uV?
Full scale of 2.1Vrms ground centers means when all zero is applied it will give the the smallest Vout which-s -2.95V and when all Ones are applied, it will yield 2.95V. Similarly for a mid code (10000.....0000) it should yield 0Volt.
00000.......0001 is one LSB , so whatever you have calculated to be your LSB then this code will be equal to that.
you can find this equation in any EE text book:
LSB= Vref / (2^n -1)
Regards,
Arash
Some devices use 2's complement, so I checked.
Thank you for letting me know that PCM5102A is not 2's complement.
Also, as I asked in the first question, this time we will use 24 bits, so I understand that 0.35uV per LSB is fine.
I understand that the output voltage Vout when using PCM5102A at 24 bits can be calculated using the following formula:
Vout=0.35uV*(code)-2.95V
Please let me know if I'm wrong.
VP-P=5.95 ( based on FS of 2.1Vrms)
assuming the channel length of 24 bit, then LSB= 5.95 / (2^24 -1) =35.4uV. if you are using a 32bit channel depth, then replace 24 with 32 and find the new LSB. If you use a 32bit channel depth but your data is 24bit, it will be padded with zeros.
The output is code x LSB
Regards,
arash
Sorry, I made a mistake in my calculations. For 24-bit inputs, 1 LSB is 35.4uV.
Also, the output voltage when set to 24-bit width is as follows.
Hexadecimal notation
code output level
0x000000 → -2.96V
0x800000 → 0V
0xFFFFFF → +2.96V
Is there a difference in understanding?