This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1754: Gain error

Part Number: PCM1754
Other Parts Discussed in Thread: TAD5112, TAD5242

Tool/software:

I'm puzzled about the origin of gain error in these devices (the whole Audio DAC family, not just the 1754). I would have expected it to be a lot smaller. ±2% seems a lot for a digital device - so I must not be understanding where it comes from.

If I wanted to best gain error, which audio DAC should I choose? Or do they all work the same way and have the same error mechanism?

I would like to use it to generate the 50Hz reference for an inverter, and I need some accuracy so that devices can be connected in parallel)