Other Parts Discussed in Thread: CC8531, PCM5310
Dear Ti,
I am currenly using CC85XXDK ( CC8531 with AIC3101 codec ) as a Master and trying to establish an upstream microphone communication with two slaves which are CC85XXDK-Headsets ( CC8531 with AIC3204 codec), I have tried using the TI-purepath configurator and could able to pair the master with two slaves. when listening through the HP output of master, i could hear only one microphone's signal, even though the second slave is paired, the microphone signal is not heard.
Can you send me the configuration files for the same ?
Also, i am trying to establish the same concept with a master containing AIC34 codec for establishing upstream with 4 slaves ( CC85XXDK-Headsets ( CC8531 with AIC3204 codec)).
Can you send me the configuration files for the same too ?
Thank you,
With best regards,
Winnefred K