Other Parts Discussed in Thread: PCM2902
i know there is no way (execpt at rom mask level) to change the USB terminal type from 0x0201 (microphone) to something better for my application... like (0x701) Radio Receiver, heck even a line in would be better
0x201 causes windows vista and windows 7, to make it the default recoding device on initial plugin
terminal type 0x0201 doesnt even make sense when somone would use the SPDIF in, no mics are SPDIF :)
I would also love to disable the output interface... so that doesnt even show up.... (and take over playback device on WINDOWS on inital plugin)
im basicly using the 2902 as INPUT ONLY for hd radio receiver (after setting up windows, it does work great)
Question... it doesnt seem documented, two pins SEL0 and SEL1 (what do they do?, if anything)... would be cool if could have it set some defaults... how about sel0 disables OUT ENDPOINT TERMINAL
oh it would be great if this IC had a full eepom (with not just VID/PID, but other settings for dsabling output or input(some people only use it for speakers!)
oh another thing, on XP, the device enumerates with NO level or mute control avail... for the input terminal, very odd...
thanks!
mitch