Other Parts Discussed in Thread: OPA353, PCM2906C
Hi,
I just finished mounting a PCM2906C and OPA353 based ADC, I'm using the USB Bus 5V power,
complete schematic:
The Codec is regularly 'seen' by my Windows 7 laptop, I can record audio,
but I get a terrific audio quality: there's an annoying digital repetitive noise, I tried to record a sweep,
here's the recorded WAV file (stereo 16-44.1, but I recorded only Left Channel).
The less noise part is without the source connected, more noise when source is connected.
In a word, I get an intermittent noise, which modulates my sound wave,
here's a shot of the recorded WAV file:
This way, the codec is not useable at all.
I've also tried to remove the uA78M33 to see if it was the cause of noise, but the result is the same.
Note: the HID0, HID1, HID2 pins are left disconnected (floating) in my design, while in the evaluation board, they're pulled high through 1.5k resistors. I'm not sure if this affects the correct operation mode.
Any idea on what's happening?
Thanks in advance.