Hello,
I urgently need to figure out the precise behavior of the dual-band DRC inside this TAS5717 amp.
First, from what I've read in this forum (and unlike what the datasheet says) the ratio and offset are fixed for a limiter-like behavior. What are those fixed values? Infinite ratio and 0 offset?
Then, and most importantly, how to tune such limiter? The compression gain is applied before the level detection (SLOS655A p4), a bit odd to me. So a soon as the input level goes above the threshold (and with given attack time constants), the compression is applied and the input level gets lowered to a value close to that threshold. With a broadband signal, this is likely to go below the threshold at times and therefore will release the compression, so the limiter will oscillate constantly between those two positions. Am I correct?
Finally, if the above is correct, I could not find a set of "softening filter" / "attack" / "release" that produces a nice sound output. Do you have typical values for the lower and upper band (x-over at 300Hz) with music?
Thank you!
Best regards,
Fred