This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8520 VBAT Monitoring

Other Parts Discussed in Thread: CC8520

Hi,

I have a question about VBAT monitoring of CC8520.

■PurePath Wireless Configurator 1.4.2.38665
 -> Headset Slave with Remote Volume
  -> Power Management
   -> Battery Voltage Monitoring

In my application, the value of the external resistor is 82kΩ.
Lowest measurable voltage is in the range 1.82 to 2.34V.
Highest measurable voltage is in the range 3.11 to 4.17V.

In this case,
the minimum measurable range:2.34 to 3.11V?
the maximum measurable range:1.82 to 4.17V?

Best regards,

Hirokuni Oota