Please can you provide a PCM5142 EVM SRC4392 192Khz config file (for use in PurePath Console). This is to allow me to test the EVM at SPDIF input 192Khz?
Previously you provided the info below for 96Khz only.
Thanks,
--------------------------------------------
was able to get the eval board working at a sample rate of 96kHz. The file below is a detailed description of my process:
PCM5142 Evaluation Module at 96kHz.docx
The issue with the eval board comes from the SRC not the PCM5142. Purepath Studio does not properly set the registers of the SRC. After setting the registers with the following file (I used Purepath Console) the PCM5142 had no issues with a sampling rate at 96kHz.
To get the eval board working set the registers of the SRC with the following file.