Hi.
I am reading data from PCM4220 through TMS320C6745.
I have the next configuration:
1) PCM4220
- Master mode
- Double Speed mode
- Classic filter response
- SUB0 = 0 and SUB1 = 0: Sub-frame 0
- OWL0 = 0 and OWL1 = 0: 24-bits
- FMT0 = 1 and FMT1 = 0: I2S
Audio serial port bit clock - 6,14407 MHz
Audio serial port left/right word clock - 96 KHz
Master clock - 12,2881 MHz
2) DSP
Codec connected through McASP.
Master clock - 24,576 MHz (Is it correctly ?)
My problem:
1) I connect VINL-, VINL+,VINR-, VINR+ pin to the ground.
But my received DATA in the buffer are the next:
I don't understand why values do not match:
866304 and 4293863168
4293863168 and 851712
851712 and 459264
etc.
Values should strive to zero, but I have values 4293863168. Why?
Your help will save me a lot of time.
Thanks.