This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LM4765 has gone obsolete. Is there a FFF replacement? I found the LM4766 but it looks like the mute circuit is different; it wants to be pulled low to the negative rail (-12V) vs the LM4765 which conveniently pulled up to the positive rail. I was controlling the LM4765 mute from the processor (+3.3V ) through a FET buffer. Do you have a recommended application circuit to interface the the LM4766 Mute pin with ( VEE reference of -12V) to a processor referenced at +3.3V?
Thanks