This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI’s class-D power amplifier solutions for high-end audio

Other Parts Discussed in Thread: TAS5630, TAS5631, TAS5518, TAS5508B, TAS5028, TAS5504, TAS5086, TAS5504A, TAS3308, TAS3108

I am posting to ask for help in narrowing down the many class-D amplifier solutions TI offers. Normally I would use the design guides and selection tools on ti.com to get my answer but in this case they seem to lead me in circles or to parts circa 2002 I wonder about using in a new design. I am also suffering from a head cold which has knocked about 30 points off my IQ (temporarily I hope) and this project needs to get going regardless of my sorry condition.

I am designing under a non-disclosure agreement so I will not reveal the application details and market this amplifier will serve. For the sake of discussion here on the TI audio form one can think of the requirements as an amplifier for a self powered hi-fi speaker with audiophile sound quality AND a power bandwidth to 100k Hz. The above audio bandwidth requirement obviously one the class-D amps only occasionally address. Reading the posts in the audio form and its FAQ I saw few addressing the high-end audio market so perhaps this topic will be of interest to others.

Primary must have requirements:

-          High-end sound quality, THD+N circa 0.01% at rated power

-          Dynamic range circa 100 dB

-          Power range 100 to 600 watts @ 8 ohms

-          Current output sufficient for 4 ohm loads, 2 ohm support desirable

-          One to four channels on PCB

-          Greater than 20kHz frequency response, preferably to circa 96k-120k range

-          Reasonable design cycle, reference designs and evaluation boards a plus

-          Digital inputs supporting up to 192k/24 bit data, analog inputs optional but desirable

 

Secondary like to have requirements:

-          Volume control in digital modulator OR by adjustable power rail

-          Ability to implement speaker crossover filters in digital domain

-          Simple HW control so microprocessor  not required

 

So, what is the short list of parts to evaluate given the above criteria?

 

Thanks

 

Norman Tracy

Audio Crafters Guild

  • Norman,

    Those are pretty tough specifications to hit. I can't promise to hit everything with one part, but there is one particular part that comes to mind.

    I'd have a look at the TAS563x devices. The TAS5630 is an analog input part, the '31 is a PWM input part.

    THD is down around 0.03% (if memory serves) and output power is up to 600W (at 10% THD... well above 300W for 1%)

    The easiest part to get into and prototype is the analog input part - the TAS5630.

    My only concern is the the power bandwidth up to 100kHz. The '5630 with the standard LC filters we use on the output can handle up to 73kHz. I believe we can push a little higher as well, but all the way to 100kHz may cause the part to struggle.

    Have a look at the datasheet, and let me know what you think.

    Cheers, Dafydd

  • Hello Dafydd & Forum readers,

     

    Thanks for the quick response last Thursday. I have reviewed the TAS563x devices and they do look promising for this application. I find it very clever how the TAS5630 analog input and TAS5631 digital input versions are pin compatible on 41 out of 44 pins on the DKD packages. I was disappointed the TAS5631 lacks an evaluation board. That is what led me to check the common pin outs between TAS5630 and TAS5631 and hatch the following scheme to quickly get an evaluation circuit online.

     

    Hack the TAS5630DKD2 Evaluation Module by:

    1.     Replace the TAS5630 with a TAS5631, account for the needs of pins 14, 15, & 16; and

    2.     Break in to the INPUT_x nodes (pins 6, 7, 12, & 13) at the inline resistors between the TAS5630DKD2 board’s input op-amp stage and TAS5630 footprint. The analog input stage is thus disconnected from the TAS5630 footprint. We’ll use shorting pins on the analog input jacks to keep the abandoned in place op-amps quiet.

    3.     Connector (to be determined matching front end to be selected) now connected to the TAS5630 footprint pins 6, 7, 12, & 13.

    Now one has a TAS5631 equipped PCB ready to connect to a TI Digital Audio PWM Processor presumably from the TAS5xxx family. Using the ti.com select page for the Digital-Input PWM Controllers limiting to 192k Fs max for this application’s requirement nine devices are offered TAS5010, TAS5012, TAS5028, TAS5028A, TAS5086, TAS5504, TAS5504A, TAS5508B, and TAS5518. Among that list I would tend to short list the TAS5010 and TAS5012 because they are 2 channel outputs matching the specification and the TAS5518 because it is listed as having the highest dynamic range. Am I correct in noting all of their evaluation boards include power amp stages like the TAS5028-5122C6EVM? Is there a PWM Processor evaluation board minus the power amp stage one could use with the TAS5631?

     

    I also spent time looking at the TAS3xxx audio processors. The TAS3108 looked great until I realized it lacks the PWM outputs needed for TAS5631. Looks like TAS3308 is the only one with PWM outs and it’s Fs maxs out at 48k, a deal killer. But it does have the TAS3308EVM a quite nice evaluation board.

     

    Comments please, have I missed the PWM Processor that supports 192k inputs to PWM outs and has an evaluation board? Or is my application too niche and its time to design my own TAS501x to TAS5631 PCB?

     

    Enough for now, regards,

     

    Norman Tracy

    ACG

  • Hi, Norman,

    We are in the process of releasing a TAS5631 EVM that will contain a TAS5508 for PWM generation.

    If you can wait, I suggest you do, fly wiring PWM signals can be a bit tricky...

    I wouldn't suggest using the TAS501x devices, I don't think they will meet your audio requirements. They are quite old, and our newer devices have better performance. The pity is, you have to buy a multi-channel device for your stereo application. You may find the newer devices are cheaper, anyway.

    -d2

  • Don, I have a 5630 EVM. I'm  very, very interested in '31 EVM. When might we see these and can you provide any advance info.  What will the board have for inputs (S/PDIF, analog etc) Will there be USB for the DSP control also?

     

    Cheers...Doug

  • Doug,

    The TAS5631 EVM is going thru the release process right now. I expect it will be available in a few weeks.

    Attached is the preliminary users guide for it.

    -d2

    TAS5631DKD2EVM User's Guide (1.00).pdf
  • Doug,

    I am happy to report the TAS5631 EVM is now released!!!!

    http://focus.ti.com/docs/toolsw/folders/print/tas5631dkd2evm.html

    -d2