Other Parts Discussed in Thread: CDCLVC1102, SRC4192
Hello,
I have a question regarding I2S audio routing within a design around PCM9211.
The PCM is used as multiplexer here.
There is one output device (an I2S input class D amp) on the PCM's main output.
There are two input devices: one on the AUXIN0 port, another on the AUXIN1 port.
The output device is a I2S receiver in clock slave mode.
The input devices are I2S transmitters in clock master mode.
From the PCM9211's datasheet I understand this setup is ideal, right?
Now, the second source device, has also an I2S data input which I want to use. There are however no seperate clock lines for this input, the same as for it's output must be used.
My goal is to make a route possible for audio comming from source 1 to the source 2 device input.
Since the PCM has multiple outputs (AUXOUT), which can be independent from the main output, I was thinking to use the PCM MUX for this as well.
However: I read in it's datasheet AUXOUT can only operate in I2S clock master mode.
Problem: The source 2 device is already master...
Is there something I missed out and is there a way to use AUXOUT or another output to accomplish this audio route?
If no: what is the best alternative?
The PCM9211 is tremendously versatile, so I believe it's possible in some way, but I'm not sure.