This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4861: When a sound is played, a noise is detected at in the initial part of the sound.

Part Number: LM4861

Hello.

We develop a system, including the audio amp, LM4861.
There is a sound noise issue related with the LM4861.
The sound noise is detected in the following cases.

1. After the audio codec output signal is input to the LM4861, and then the LM4861's shutdown pin becomes Low(low active)
2. After the LM4861's shutdown pin is Low, and then the audio codec output signal is input to the LM4861.

I have mentioned in detail this issue in the attached file.

Thanks.

alc5621_amp circuit.pdf