Part Number: PCM1792A
Other Parts Discussed in Thread: OPA1612, OPA2227, PCM1794A
Hello,
I am using the PCM1792A in monaural mode. I am experiencing a very steep rise of the distortion on only one of the side of a given DAC. For example, the plots below shows in blue the output of IOUTL-and IOUTL+ for both the THD+N level and ratio, where as the red plots show the same datas for the IOUTR- and IOUTR+. As a result, the THD+N ratio @ 0 dBFS input is ~111 dB on one side of the DAC and -97 dB on the other side. As the device operates in monaural, both sides are supposed to process the same input data which is in this case a 1kHz signal with the input level ranging from -30 dB to 0dBFS. What can cause such a different behaviour between channels on a single IC?